This directory contains all the images required in the boot partition of the boot media.
- tiboot3.bin (and sysfw.itb if applicable)
- tispl.bin
- u-boot.img
- uEnv.txt

There will be multiple variants of the bootloader corresponding to the SOC variant supported by that
binary, while the one in use will be named simply tiboot3.bin (and sysfw.itb if applicable).
- tiboot3-<SOC>-gp-evm.bin    ( and sysfw-<SOC>-gp-evm.itb )    : Used for a GP device
- tiboot3-<SOC>-hs-fs-evm.bin ( and sysfw-<SOC>-hs-fs-evm.itb ) : Used for a HS-FS device
- tiboot3-<SOC>-hs-evm.bin    ( and sysfw-<SOC>-hs-evm.itb )    : Used for a HS-SE device

For example if using a HS-SE device for an SOC, simply replace the tiboot3.bin (and sysfw.itb if
applicable) before trying to boot the device:
    'cp tiboot3-<SOC>-hs-evm.bin tiboot3.bin'